Part Number: LM358
Other Parts Discussed in Thread: LM7321, TL052, LMV358, THS4052, TLV172, MC1458, TLC072, LM7322
Hi,
I am using LM358 OPAMP to amplify 3.3V to 12V. This OPAMP capable of giving output current of 20mA.
New requirement has come load current increased to 40mA
Now I am looking for replacement for LM358 OPAMP with higher output current. Preferably same package.
Below is my requirement.
- Single Supply voltage +15V
- OPAMP should be capable of giving 40mA output current at full operating condition
I have looked into LM7321. In datasheet output current is not clearly mentioned for full operating condition.
can anyone suggest alternate OPAMP for LM358.