Part Number: OPA4140
Other Parts Discussed in Thread: CC2541, , TPS65133, TINA-TI, OPA137, OPA140
Tool/software: Code Composer Studio
Dear TI officer and members,
Currently, I am using the CC2541 to collect an analog signal.
The amplifier of OPA4140 was adapted as shown in the listed figure.
Here is the problem that the OPA4140 is every hot (close to 80 C in the ambient environment of 25 C) due to the large input current of 120 mA, which is overcurrent.
This is impossible under the normal condition. I can not find the reason. Please help me.
The positive and negative voltages are provided by TPS65133 dual-output supply.
Best regards,
Derrick