Other Parts Discussed in Thread: TINA-TI, , THS4031
Tool/software: TINA-TI or Spice Models
I am simulating a differential amplifier that uses composite amplifier techniques using an OPA1611 and THS4031, and I am looking at the step response stimulating using a 50Hz square wave and simulating from 9.999 ms to 10.001 ms to look at time domain response.
The model has been simulating just fine, but I tweaked some values, and now the simulation will not complete. It hangs at the 90% level. The preview button does not display any useful information, inly displaying a since vertical line from -730u to 590u at 9.01 ms (which should not be part of the simulation).
How do I trouble shoot these types of issues in TINA-TI?