This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4552: High Pass problem

Part Number: THS4552

Hi,

i am having an issue using the THS4452 as a high pass filter.

I designed the high pass filter with FilterPro from TI and here is the schematic:

My schematic looks like this : Power Supply +5V and GND and VCOM is 2,5V

The problem is that the Opamp is drawing 140mA current. Once i take the C62/C61 and C16/C17 its not drawing almost any current.

Is the Opamp instabel? Is it oscillating?

Obs: Low pass filter is working fine, i have 4x THS4552 as Low pass fitler configuration.