Part Number: THS7530-Q1
Hi,
Data sheet of THS7530-Q1 page7 Please tell me how to look at Figure2.
When VG+ = 0V , Gain is 11.6dB (typ)
When VG+ = 0.9V, Gain is 46.5db (typ)
This is described in datasheet page5.
This value is a reference value, I understand that it is not guaranteed value.
(As it is typ)
page7 Looking at Figure2
When VG+ = 0V , Gain is about 7dB (typ)
When VG+ = 0.9V, Gain is about 41dB (typ)
And you can judge by looking at the graph.
When VG+ = 0V , for the reference value of 11.6dB,→ 7dB in the graph of Figure 2
Also
When VG+ = 0.9V, for the reference value of 46.5dB,→ 41dB in the graph of Figure 2
Q1.Why is there a big difference?
Q2.Also, the gain error is shown in Figure2 with Gain Error, but will Gain-Error fluctuate due to temperature change?
Q3.How is the individual difference (variation) of Gain-Error?
Q4.How is the individual difference (variation) of Gain?
best regards