Part Number: OPA4377
Other Parts Discussed in Thread: OPA377,
Hi
It is mentioned on the datasheet that the input terminal has a clamp-diode.
So that ,the absolute maximum rating of the input terminal is defined as bellow.
1. Is this spec same as the common voltage range of differential input?
2. And "0.5V" of the above maximum rating is Vf voltage of clamped diode?
3. Is there any clamped diode between +IN+ and -IN?
Best Regards,
Koji Hamamoto