Part Number: AMC1200
Hi Team,
In the datasheet of AMC1200, it specs the offset error is 1.5mV max. I am wondering how do you test the offset. Short VINP and VINN, then measure output?
in terms of the output common-mode voltage, it specs 1.29V when VDD is between 2.7V and 3.6V, 2.55V when VDD is between 4.5V and 5.5V.
my question is what is the common-mode voltage when VDD is between 3.6V and 4.5V.
Regards!
Yangbo