This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ACF2101: Application question for single channel mode

Part Number: ACF2101

Hello,

I have some questions about ACF2101 that I must use in my project for studies that I can not find in datasheet. 

1) If I want to use single channel (for example channel A) of this OP AMP what should I do with second channel to get the best performance? Should I short the input pins to the ground and output left open? Or I should leave all the pins open from channel B? 

2) I will not use multiplexing in my application, should I then connect "SW Out" and "SW Com" to the Low logic lever or high? The output voltage in this scenario will be at "Out" pin? 

Best regards,

Bartosz