Part Number: INA181
Other Parts Discussed in Thread: INA138, INA139,
Hello.
Can I add an input resistance to the INA181A1 and set the gain to "10"?
By Page-25 of SBOS793D.
When RF is added to the input, the gain shifts.
Gain = 20 = R2/R1
R1=25kΩ
R2=500kΩ
R1 is the input side of internal resistance.
R2 is the output side of internal resistance.
When RF=25 kΩ is added to the IC input side, will the gain be "10"?
R1=25kΩ+25kΩ=50kΩ
R2=500kΩ
Gain = R2/R1=10
Regards,
Dice-K