This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12Vin 5Vout @ 40mA max regulator, +/-20V tolerant on output

Other Parts Discussed in Thread: TPS7A4201

hi,

I'm looking for a power amp to supply a Nordig device (STB app).

Input is 12V +/-15%, output 5V +/-3%, max output current 40mA, max load 100uF, w/ EN, and must be +/-20V tolerant on the putput pin/connector...

we have a solution w/ discre components (lots of R, diodes, etc.) so was looking for something cost effective (like an opamp) but that could allow space saving (smaller BOM)...

thanks a lot in advance

KR

Vincenzo