Other Parts Discussed in Thread: TLV1704
Dear Sir, please answer
We use LM2901 in power channel of traffic light controller. Please see attach.
LM2901 is used to monitor the signal level on a R9 resistor.
If there is a short circuit, there can be a large voltage - 40....80 V on a R9 for a time 10 mS - (until the protection goes off and the triac control signal is not turned off)
The LM2901 often breaks down during short circuit - protection in the form of VD5, VD6, VD13 does not help. Rather helps, but badly. I want to clarify that the voltage control on R9 is not done to determine the short circuit. If everything is normal, then a current of 50...200 mA flows through the R9.
Can you advise how to improve the protection?
Sincerely,
Vladimir Naumenkov
www.agat.by