This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA282-Q1: about input bias current

Part Number: INA282-Q1


Hi team

INA282-Q1 D/S say Input bias current = TYP 25uA per pin.

so total input bias current would be TYP 50uA(= 25uA x 2) for two input pins ?

further, may I know total input bias current for  two input pins at Vs = 0V and common mode voltage = 20V ?

  • Hello Paul,

    Thank you for your interest in our INA282-Q1. The input bias current in the datasheet corresponds to the average value for both inputs, so the max will be 50uA for Vs=5, Vcm=12V.
    For this device architecture, we expect the input bias current to basically be 0 for Vs=0V.