Part Number: LMV761
Dear E2E member,
I want to know the differential input which is IN+ - IN-, the maximum rating is 5.5V, right?
Is it OK for this design as below?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMV761
Dear E2E member,
I want to know the differential input which is IN+ - IN-, the maximum rating is 5.5V, right?
Is it OK for this design as below?
Dear Kai,
Thanks for you reply.
I still want to confirm some questions.
1. Now 3.9V sequece always prior than 3.3V. So What can we do in this design? Do we need to change others part?
2. If over CMVR, what the issue does IC happened?
3. What the CMVR SPEC at VCC=3.3V of LMV761?
Thanks!