This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM339A: Maximum load capacitance value

Part Number: LM339A


What is the maximum load capacitance (Cload) value for LM339A that Output pins OUT1, OUT2, OUT3 & OUT4 can drive?

  • Hi Shashank,

    adding a load capacitance to the output of a comparator can heavily slow down the output slew rate and increase the propagation delay times. This is especially true for a comparator with open collector output which usually uses considerable pull-up resistances. Also, when toggling low the ouput transistor will short circuit the load capacitance which will result in a considerable output current spike generating lots of ground bounce and ground noise. Even the output transistor can be damaged due to the heavy output current spike, especially if a big load capacitance is used.

    About how much load capacitance are we talking about?

    Kai