Part Number: ISO124
Other Parts Discussed in Thread: INA146, ISO224, AMC1200
Hi everyone, this is Mike.
I have designed this circuit based on the datasheet of ina146.pdf and iso124.pdf
But I have some questions related to the ISO124
I think I have a problem in the input impedance of the ISO124 because of the INA146 feedback.
What do you think?
Also I think I'll have some problems with the signal coming with INA146 because of the ground reference, the voltage at the input, at JCA, es line to line, so it is a differential measurement, after the signal passes through the ina146 it has a ground reference. I get confused at this point.
Thanks for all your help !