1.- To calculate the "short circuit" (RL = 10R) power dissipation for this device:
Pd = Ibias*Vcc + Iload*(Vcc-Voutput), is this assumption correct? (approx..)
2.- Which pin(s) of this device can be used to sink heat this device (D package)?
I am trying to use the PCB as heat sink. (I can't use the DGN package because of foot size compatibility)
3.- The DGN package has a thermal pad, where is it connected internally?
can I connect it to GND?
Thank you
Fausto