Part Number: INA2126
Hi to all!
I need to capture two signals from two load cell, so i did a circuit with an INA2126 to amplifying this signals and acquiring they with an adc.
This is my circuit
The load cell is supplied using the REF5030 component.
The problem is that this circuit give me the same output regardless if i put a load on the load cell.
In particular, using a multimeter i measure this values for the A side of the ina:
- V+ = 3.99 [V]
- Vin+ = 1.46 [V]
- Vin- = 1.46 [V]
- Vo = 0.53 [V]
The output of the REF5030 is 2.98[V]. I use a single supply configuration with V- = Vref = GND.
For the B side of the ina, with no load cell attached, i measure this values:
- Vin+ = 0.06 [V]
- Vin- = 0.06 [V]
- Vo = 3.33 [V]
I have no idea on what is the problem and why i obtain this values in output, so please someone help me to understand why this circuit doesn't work properly?