This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2595: Maximum supply current consumed

Part Number: CC2595


Hi Community,

In CC2595 datasheet it is mentioned as maximum current consumption @ +20.7dBm output power is 98mA.

I have clarify regarding the total required current for this part during Active mode/ Normal Operation mode. only it will consume 98mA  ?

Please provide the detailed current requirement for this part.

Thanks & regards,

Divya

  • Divya:

    The CC2595 operates with Class-AB bias so the current consumption changes with output power. Min current with no input power is 30 mA. Max current at 20.7 dBm is 98 mA. Figure 2 in the datasheet shows a curve of supply current vs. output power.

    --RJH