Hi Team,
Do INA300 get IEC60950 certification?
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello SHH,
Thanks for reaching out on the forum. Although this part is recommended for computers, servers, and telecom equipment which falls under the umbrella of information technology equipment not exceeding 600V, none of our specifications indicate that they are meeting IEC60950 standards. Thus this part does not have the IEC60950 certification. For future reference you can typically find the certifications we have for the part by the front page of the datasheet. Below is an example that shows the AMC1300x has UL1577 certification: