Part Number: LMP7701
Other Parts Discussed in Thread: TINA-TI
Hi, I'm using an LMP7701 as a transimpedance amplifier with 249-kohm gain. When I apply a signal to the non-inverting terminal, I expect to see it on the inverting terminal, via feedback action--this method is often used in electrochemistry. But with this circuit, when I apply a square wave with 10-µs rise/fall times to the non-inverting terminal, I see segmented rising and falling edges on the inverting terminal--the signal tracks the input nicely for about 0.6 V, but then ramps over. I'm guessing this a slew rate limitation, but the applied dV/dt is only 0.1 V/µs, whereas the typical slew rate for the LMP7701 is about 1 V/µs (at Av = +1).
Supply voltages are ±6 V. The load on the transimpedance amp is 20 kohm in parallel with the input capacitance of another LMP7701. There's a 20-pF cap in parallel with the 249-kohm feedback resistor.
Thanks for any advice! --Chris