This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPY634: Accuracy when using MPY634 as a divider

Part Number: MPY634


Hello, I am using MPY634 as a divider. On the datasheet, it says that 'accuracy of the divider mode typically ranges from 1.0% to 2.5% for a 10 to 1 denominator range depending on device grade'. I don't understand what it means by '10 to 1 denominator range'. Does it mean the value of the denominator needs to be between 10V and 1V? Or does it mean the ratio of numerator and denominator has to be between 10 and 1? Or something else? Many thanks. Eric