Part Number: LM2904
Hi team,
My customer is using LM2904 to detect the motor current for the cordless vacuum cleaners application. As picture shown as below, the MOS is either on or off for a long period. Customer want to test the average current from AIN PIN(from a simple MCU), but the integrated AD is very slow(120k) and only have 8 bit. So they add a 10uF capacitor for the output of amplifier in order to get the average current of the motor.
Question is using this 10uF cap, I am wondering if this will cause stability problem and the response is very slow.
Do you have any suggestions for this? or a better solution?
Thanks!