Part Number: TLV3012
Does TLV3012 require a series resistor in-line with the inputs to limit the current if inputs ever go beyond the supply voltage? Don't see this info in the datasheet.
Thanks
Viktorija
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV3012
Does TLV3012 require a series resistor in-line with the inputs to limit the current if inputs ever go beyond the supply voltage? Don't see this info in the datasheet.
Thanks
Viktorija
Hello Viktorija,
If you can guarantee that the inputs will not exceed the supplies, then you do not need a resistor.
But it is recommended if the signal is coming from an off-board source, or, a source that is derived from another power supply system, that some series resistance is added to limit any transient currents that may occur during the power-up or power-down sequence.
Our rule-of-thumb is 1kohm per volt of expected overvoltage. So if the worst case is 5V, then add a minimum of 5k series resistance.
If everything is coming off the same supply, on the same board, then you do not need a resistor.