Part Number: THS4631DDAEVM
Other Parts Discussed in Thread: THS4631, OPA2810, THS4012
Is there a dual version of the THS4631?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS4631DDAEVM
Other Parts Discussed in Thread: THS4631, OPA2810, THS4012
Is there a dual version of the THS4631?
Thank you for your prompt reply!
Our criteria is:
SLew > 300V/uSec
PS +/-10V or higher
noise 8uV/rthz (some latitude here)
unity gain stable
>80MHz BW at G=1
Pkg Dual SOIC (some latitude)
Hi Chuck,
Is it necessary to be FET input?
If not, the THS4012 meets the above criteria. It is unity gain stable with a BW of 290 MHz, 310 V/us slew rate, 7.5 nV/rtHz noise, and comes in a dual SOIC package.