Part Number: LMC6482
Other Parts Discussed in Thread: OPA379, OPA376, LMP7721, OPA388
Hi team,
My application is as below:
The input signal is the nA grade current. The current is input to LMC6482 and LMC6482 is used as the transimpedance amplify. Then the output voltage of
LMC6482 is input to LT6000 that is an op amp of ADI company. LT6000 is used as the non-Inverting amplify. The datasheet of LT6000 is in the attach.
The output voltage of LT6000 is input to ADC. VCC is 3.3V for my circuit system.
Now I want to find an op amp to replace LMC6482 and LT6000 at the same time. So I think the ibias should be less than LMC6482 and the offset voltage should be less than LT6000.
I need the smallest package since my board area is very small. The op amp that is I need should be 2 channels. If TI does not have the 2 channels op amp, can you confirm if
you have one channel and the package is very small that can replace LMC6482 and LT6000 at the same time?