This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6212: Usecase of THS6212

Part Number: THS6212

Hello,

I would like you to confirm whether THS6212 can be used as two general OPAMP or not.

According to title of THS6212 datasheet, there is description of "Differential".

However, when i check function diagram of THS6212, it seems that output is NOT configured as full differential AMP.

So, it seems that user also can use this device as two single end output OPAMP.

Since there is no desciption about single end usecase in datasheet, could you please confirm whether user can also use this device as two single end output OPAMP or not ?

Best Regards,