This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7530: Clipping on high input amnplitudes?!

Part Number: THS7530

Hello,

we built up an ultrasound RX path with two THS7530 in series and are now faced with the following (ugly) behaviour. The configuration is single ended to differential, this is my input signal at pin Vin+:

With minimum gain (Vg+- = 0V -> 11.6 dB) I'm expecting a sine with around 4 Vpp on the outputs, but at pin Vout- I only get this:

The THS7530 clips my sine and I don't now why. I can't find any limitations regarding the input voltage in the datasheet, except in section "DC performance". The output clamp circuit isn't the problem, these voltages are set to 1.5V and 3.5V. By increasing the gain I get this:

Is this a known behaviour and can you reproduce this with your eval boards?

Thanks and Best Regards

Hendrik