This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: use USB2ANY.dll in own software project (Delphi)

Part Number: USB2ANY
Other Parts Discussed in Thread: DS90UB953-Q1EVM

Hello,

I have the same case,I installed the USB2ANY software. But I couldn’t find the TI USB2ANY SDK folder. I only found [USB2ANY.dll] in [c:\Windows\SysWOW64\USB2ANY.dll].

When I run [USB2ANY_SupportInfo.exe], I got the following information in [USB2ANY Explorer API Debug.log] file:

2018-08-24 09:32:01.057 DebugLogging is Enabled

2018-08-24 09:32:01.057 PacketLogging is Disabled

2018-08-24 09:32:01.057 Profiling is Disabled

2018-08-24 09:32:01.058

2018-08-24 09:32:01.058 ################################ SESSION START ################################

2018-08-24 09:32:01.058 Loading C:\windows\system32\USB2ANY.dll (v2.8.2.0)

2018-08-24 09:32:01.058 Loaded by C:\Program Files (x86)\Texas Instruments\USB2ANY Explorer\Bin\USB2ANY Explorer.exe)

2018-08-24 09:32:01.058 SDK path is 'C:\Program Files (x86)\TI USB2ANY SDK'

2018-08-24 09:32:01.127

2018-08-24 09:49:18.792 Logging enabled.

2018-08-24 09:49:18.793

2018-08-24 09:49:18.794 Unloading C:\windows\system32\USB2ANY.dll

2018-08-24 09:49:18.796 ##################### SESSION END 2018-08-24 09:49:18.796 #####################

 

 

But ['C:\Program Files (x86)\TI USB2ANY SDK] folder is not available !

is there a link where I can download the SDK and the Examples ?

Thank you for your help.

Aziz