Other Parts Discussed in Thread: THS4302, THS4304, LMH3401
Hi, My name is Netanel, i'm making a project as a student in Israel, Haifa.
I'm looking for an OpAmp which is suitable for differential to single ended conversion. the conversion is intended to be made on differential data signal which came out of a high speed voltage out DAC.
the signal frequency is 750MHz. the Amplifier OPA855 may suitable but the data sheet lacks information about linearity and harmonic distortion. Do you have such information?
In addition, my Bandwidth requirement is demanding- the signal is a data signal so the amplifier's frequency response need to be as flat as possible until 1GHz. I found another amplifiers which may comply like: THS4302, THS4304.. Are there any other amplifiers?
thanks for the help