Hello!
I am trying to convert a PWM output from a IR sensor to a analog signal. I am measuring temperature change in a system and i need a fast response time (is the us) and a very low voltage ripple : ~1mV. This is not possible with a simple RC circuit, so I was looking into active filters. My PWM signal swings from o to 3V and the period is 1.024ms. I can not increase the PWM frequency. Would the OPA187 work for this application?