This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1211-Q1: Why is the Maximum Vp-Vn of AMC1211-Q1 only 2.88V even with 5V VDD2 ?

Part Number: AMC1211-Q1


I see from the datasheet of this isolated opamp that the VCMout has only the value of 1.44V.

Does that means I can only get the maximum Vp-Vn of 1.44Vx2=2.88V?

In addition, the figure31 below also shows this phenomenon.