Part Number: INA3221
Hi,
Is there a way to disable the Power-Valid alerts in the INA3221 registers? I tried to set a negativ value (two's complement) to the Power-Valid Upper and Lower register, so that if the voltage on the IN+ inputs drops to 0 volt the alert is not triggered. According to Chapter 8.6.2.17 of the datasheet it should be possible to set a negativ value to the Power-Valid register (Bit 15 is the SIGN bit).
If I set a negative value to the register and read it back, then bit 0-2 and bit 15 are always set to zero. Is the SIGN bit in Figure 48 (Power-Valid Upper-Limit Register) wrong?
If I set the Power-Valid register to zero with IN+ inputs floating, then the Power-Valid Alert is randomly triggered, which causes interrupts on the microcontroller!
Thanks for your help in advance.
Eric