Hi dear supporting team,
when customer use OPA2171 with 3.3V single supply, they will find there is lower than -0.5V voltage showing up at Vin+ for more than 10ms. by adjusting the circuit, they could control the input current to be lower than 10mA, so want to double check with you:
1. if the current does not exceed 10mA, what' the max negative voltage it could bare?
2. if the current does not exceed 10mA, Vin+=-1V, how long time could it last without damaging the part? (or withouth causing potential damage)
tks a lot!