Other Parts Discussed in Thread: TCA9548A
Dear all,
I'm testing my own electronic designed for 3 and 4 electrodes sensors. I was reviewing the last 4 days of a OX-A431 Alphasense sensors, and it present a signal drop that tough four hours, and then the device was reset and the signal come back to the original value. It happened for both Working and Auxiliary electrodes.
I had 3 more sensors (of the Alphasense A4 series) connected to the same device, and its present the same signal drop at the Working Electrode (not at the Auxiliary) at the same time. This happened two times.
The LMP9100 works in 3-lead amperometric cell, and goes to standby between each read. Could it be that the sensor goes to sleep mode and when was reset it went to 3-lead amperometric cell?
The point A is when was reset.
Thanks in deep.