Part Number: TLV172
Other Parts Discussed in Thread: TLV1805-Q1, OPA197, TLV9062, TLV1805
Hello,
Our customer are searching for a single logic buffer.
They need a 18V operation, handling 40kHz square wave, push pull output, mounted in a small package and low cost.
I found the TLV172, have a question.
There is the back to back diodes between IN+ and IN-.
When the customer use the TLV172 as a comparator, a current flow through these diodes.
The customer use the external resistor as 100kohm. So the input current will be less than 10mA.
Is it possible to use the TLV172 as a comparator?
Best Regards,
Naoki Aoyama