This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
This is Gordon Liu of WNC in Taiwan.
I want to use OPA2674 be a RF PA at 13MHz.
I use the below test circuit ti test it and I got OP1dB is only 19dBm but datasheet show the max output current is 350mA.
Could you teach me where wrong is??
PS: Load=50 ohm that is spectrum analyzer
BRs,
Gordon Liu
12V DC_In (mA) | Pin (dBm) | Pout (dBm) | Gain (dB) |
30 | 0 | 12 | 12 |
32 | 1 | 13 | 12 |
32 | 2 | 14 | 12 |
34 | 3 | 15 | 12 |
36 | 4 | 16 | 12 |
40 | 5 | 17 | 12 |
42 | 6 | 18 | 12 |
44 | 7 | 18.6 | 11.6 |
46 | 8 | 18.9 | 10.9 |
48 | 9 | 19.1 | 10.1 |
50 | 10 | 19.2 | 9.2 |
Hi Gordon,
I've also noticed that you asked the same questions in the thread listed below. I am going to close that thread, please ask any further questions in response to this thread.
e2e.ti.com/.../727640
Regards,
Jacob