Part Number: OPA2674
To whom it may concern,
I have these questions:
1) Are the specs listed on the data sheet for 1 of the 2 op-amps or 2 op-amps working together?
2) If I want to drive a 10ohm Rload with 0-5V swing, can I use +6V as V+ and -2.5V as V-?
3) If the answer to the first question is 2 op-amps working together, can you really put two op-amps in parallel for more output current?
Thank you.
Weiyu