This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: ina240

Part Number: INA240


Hello Team,

In the INA240 product folder there is a error calculation tool which is useful!

But I would like to have current range from 0.1A to 130A and the tool only supports up to 100A.

My system specs are shown below:

1. Rshunt: 0.1m-ohm

2. Load current: 0.1A to 130A

3. Operating temperature 60 degree C

4. High side sensing 12V Vbus

Could you share INA240A4 error calculation excel file with me so that I can change the load current to 130A and check the error%?

Thank you.

Regards,

Lynn