I am currently trying to specify the sampling rate of an external ADC measuring the voltage of the LM2907-N for a legacy design. (I understand that this is not the most efficient method of doing things, but this is the required architecture)
According to the LM2907-N datasheet (SNAS555D –JUNE 2000–REVISED DECEMBER 2016) section 9.1:
"C2 acts as a filter to smooth the pulses of current and does not affect the output voltage. However, the size of C2 determines both the output response time for changes in frequency and the amount of output voltage ripple."
however the datasheet never mentions how to calculate the response time of the circuit. Should I assume it is limited by the time constant t = R1C2?