Other Parts Discussed in Thread: OPA171, TLV2370
Hello to the Ti community.
I have been spending some time with the selection tools, but can't seem to find something that fits the bill and am hoping for some advice on a good part or two.
First of all, it needs to be small. SOT-23-6 would be the largest that could be considered, and smaller would be very desirable. Any type of WCSP is fine; the smaller the better.
Single opamp device
Single supply that can operate at 15V or higher
Input must go down to V-
Slew rate of at least 0.4V/us, preferably 2 or higher
Lowest operating current that will support the above (will consider some trade off with SR)
Able to source 20 mA (not continuous, power dissipation should not be a problem)
Low offset would be nice
And now the thing that seems to kill all of the selections. I want a logic level low shutdown pin.
If such a part doesn't exist with the low shut down, we could consider a logic level high shutdown but the current into that pin would need to be minuscule. Or, if no shutdown pin at all, it would need to have very low Iq and, with the inputs at V-, not output any current as the V+ rail decayed down to zero (which is something that I can't determine looking at the datasheets).
Much thanks to anyone that can point me in a good direction.
Brian