This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey
I've created my first PCB design
using the design from http://www.ti.com/tool/TIPD181 as a basisfor the quad channel preamp OPA4172.
circuit wire up:
https://imgur.com/1e0fYMw
Pcb Design without ground plane showing:
https://imgur.com/DmMtIYb
Pcb with ground plane:
https://imgur.com/5kgW2RJ
My issue is that all my inputs (mic 1-4) are all showing up across all outputs. Eg; mic 1 will show at all outputs, 2 at all outputs etc etc.
I've tried making another circuit with no ground plane in the case that the PCB tracks were crossing with the outputs but it sounds awful and still has the same issue.
Thanks
Hi Andreas,
please don't feel offended, but the layout is highly disadvantageous. :-)
You should move the components much closer to the OPAmp. This is especially true for the decoupling caps and filtering caps. You should avoid long copper traces and minimize loop areas. And last but not least, you must strictly separate input and output lines.
If you use microphones with cabling, take shielded cables and connect the cable shield to signal ground.
Again, what microphones are you using?
Kai
Fair enough i was hoping that there would be another reason on this weird crossfeeding.
I've got 4 individual ones ,although through-hole variant so that should cover me till i order the soic ones in.
Thanks for taking the time to answer my query !
Hey Sorry i didnt answer your prior question
Im using a cmi-5247tf-k
dont pay attention to that 1uf cap as thats was a mistake
Hi Andreas,
Here are a few blogs I've written on PCB layout of an op amp to help in the next revision of your PCB.
The Basics: How to layout a PCB for an op amp
How to layout a PCB for high-performance, low-side current sensing designs
Kai is correct in that long cabling can effect the stability of the amplifier so I recommend either connecting the microphone to the PCB or changing the feedback capacitor to ensure the amplifier is stable with the cable capacitance included in your design.
Thank you,
Tim Claycomb
Sorry, i had just checked my image that i had attached at the start of the post and had noticed i attached the wrong image.
For some reason my feedback resistor should be 12p, along with r4 and c6 being 50 olm and 2.2uf respectfully.
Either way i appreciate the assistance, i resolved the issue using 4 separate boards until i can produce an ideal board
Regards
Andreas
Hello Andreas,
Is the feedback cap R2A-D really 2.2uF?? Compare to the reference design...it should be around 20pF.
If so, most likely that is your problem. There are many things going wrong if this is the case - mainly the various mic signals are sneaking around the amplifier and the "other" amps are back-driving the signal path.
Remove the 2.2uF C2's and replace with a few pF and it should work.
Also - increase the size of C1. The microphones have very low supply rejection (PSRR) - so any "modulation" of the supply will appear on the inputs slightly attenuated.
Hi Andreas,
I would use the following scheme:
This scheme allows a somewhat longer microphone cabling. Also, the supply voltage of the electret microphone is filtered. This can considerably stabilize the amplifier, as Paul already mentioned.
Kai