Part Number: LMP8646EB
Other Parts Discussed in Thread: LM3102, LMP8646
Hi, I'm working with LMP8646EB evaluation board suggest from TI engineer Amy Le with his very interest video, anyway connect and test the board something seem not to work properly.
The problem is that the LM3102 (or LMP8646) do not limiting the current to the super capacitor that goes over his 2.3 volt limit... dangerously !
These are my questions:
1) Are the evaluation board ready to use out of the box with all correct components for the supercap installed ?
2) Why the User guide suggest to use a second power supply for the LMP 8646 V+ ( the LM3102 itself provide the Vcc to LMP8646 via JP1 )
3) There is need to connect J2 VP ?
Thank you
Massimo