Part Number: TLV6710
Other Parts Discussed in Thread: TLV6713,
Datasheet, April 2018, indicates absolute max VOUTA, VOUTB +28 V but in other places it suggests VOUTA, VOUTB nominal to be 36V. Which is correct and should absolute max = +40V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dan,
The TLV6710 and TLV6713 outputs can be pulled-up to 25V (28V Abs Max) regardless of supply voltage.
The datasheets have been corrected and will be going through sign offs for release. Hopefully the corrected datasheets should be on the web in a few days. Revision history is now part of the datasheet standard.