Part Number: LMP8358
Other Parts Discussed in Thread: ADC141S626
Why is the LMP8358 limited to 100mV differential input? I would like to use it to 150mV or even 200mV. I see the absoulute max input is limited to the rails. I am suppling the INAMP with 5V and -0.3V. I'm using it to sense current loside (0 to 200mV ) above circuit ground.