Hi all,
I am using OPA2209, powered by +/-15V
The two op-amps on OPA2209 are configured as unity gain follower
Both input+ are connected to ground
I measure the difference between the two outputs. I will accept a constant small DC difference
Unfortunately, I observe the voltage difference between the two outputs is like a charging-style DC-drift as the circuit warms up. When I place the circuit in the fridge, there is a discharging-style dc-drift.
It takes about an hour to settle and and total dc-drift is around 300uV, way higher than the spec of the op-amp.
Any suggestion on how to minimize this?
Thanks for any pointer!