This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET8551T: Input Referred Noise Charts

Part Number: ONET8551T

In the datasheet under AC Electrical Characteristics, the Test Condition for the Input Referred Noise is 10-GHz bandwidth.  Is there a chart or data that shows the magnitude or values of the Input Referred Noise over the 10-GHz bandwidth.  What I am trying to determine is what is the noise in the lower frequency range of 100kHz  to 600MHz.  I have calculated the NEP(noise equivalent power) and need to know the variation over frequency.