This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4532: Looking at the above circuit design is reasonable?

Part Number: THS4532


Dears:

Customer wants to use THS4532 to realize single signal to differential signal. In the below figure, A is a sinusoidal signal with a midpoint of 2.5V peak-to-peak value of 300MV. A+, A- want to get a differential signal with a midpoint of 2.5V peak-to-peak value of 1V. Please help us. Looking at the above circuit design is reasonable?

Is the THS4532 selection reasonable and is there a more suitable chip? Need 2 differential amplifiers.