Other Parts Discussed in Thread: AMC1302EVM, AMC1300, AMC1301, ISO224, AMC1302
Dear TI Members,
Does anyone have experience with this Evaluation Board ?
AMC1300EVM
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Members,
Does anyone have experience with this Evaluation Board ?
Thanks
Yes I have bought AMC1302EVM,
Any suggestions for handling the input ?
Do I need a voltage divider for it ?
I want to detect 240AC and feed the result to ADC,
Thanks
Hello Collin,
Thanks for your comprehensive answer,
For AMC1302EVM, I can use the same guidance while using AMC1300 ?
How about the resistor rating ?
Will 1W rating resistor good enough for 240V AC ?
From datasheet I can see on AMC1302, it has
"±50-mV Input Voltage Range for Low Dissipation,
Shunt-Resistor-Based Current Measurement"
Thanks