Other Parts Discussed in Thread: OPA657
Hi, we're building a fully differential amplifier circuit using two OPA657 as the front buffers. It has some problems and while checking things out, we decided to look into the input impedance of the OPA657. The specs say it should be 10e12 ohm which means "open" on our Fluke 115 multimeter. However, out of 10 chips we have, 7 showed "open" while 3 showed ~ 30Mohm. Why is that? Does that mean there is some problem with the 3 chips showing 30MOhm?
Thanks,
Jay