This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA301: OPA 301 Issue

Part Number: OPA301

Dear all,

I am trying to build a simple filtering stage for baseband signals. Therefor I use an Opa301. The Problem is that when I want to filter a sinusoidal signal with a DC offset of 2.1V and amplitude of 100mV something strange happens if my power supply is 3 V. However when I increase the voltage of  Vcc, eg to 5V, the problem vanishes at some point. Of course, by using an ideal OPamp, this behaviour doesn't occure neither.

Can somebody give me a hint?

Thank you a lot in advance!

Best regards,

Ben

TIUpload.TSC